Technical FAQs

Ask a Question

What is the difference is between a QO13842MX225 and a QO13842UX225, Intelligent Load center?

Product Features

Product Line:

Clarifying product feature differences

The QO13842MX225, Intelligent Load Center comes with a 225 Amp Main Circuit Breaker installed. The QO13842UX225, Intelligent Load center comes with `Studs only` to mount any circuit breaker up to 225 Amps. These Intelligent load centers require a special Main Circuit Breaker which is a QOM2 * * * VH-8041. The 8041 is the adder of a fast tab for control wiring to a transfer switch.

CTA-ID : 2030027
Was this helpful?
What can we do to improve the information ?