Technical FAQs

Ask a Question

What is the number of terminations available on FAL Circuit breakers?

FAL Circuit Breakers are designed for 1 conductor per phase.
With special-purpose Power Distribution Connectors for UL508 Industrial Control applications, up to 6 conductors may be terminated on the Load end.


CTA-ID : 2030025
Was this helpful?
What can we do to improve the information ?