Technical FAQs

Ask a Question

What is the part number for the ATV58 115 VAC I-O card?


The module is compatible with the control terminal strips used on V5.1 IE32 control boards and newer. This control terminal strip version has 10 terminals, including an analog output, AO1. The module is not compatible with earlier, 9-terminal strips.

The Instruction Bulletin is part # 30072-450-80.

CTA-ID : 2015861
Was this helpful?
What can we do to improve the information ?