Technical FAQs

Ask a Question

Do we offer a pendant station that is rated NEMA 7 & 9?

Issue:
Do we offer a pendant station that is rated NEMA 7 & 9?
Product Line:
Pendant Stations                            
Environment:
9001Type BW Pendant Stations
Cause:
Application is calling for Nema 7 & 9 pendant station.       
Resolution:
No pendant station are Nema 7 or 9 rated, only offer control stations.
Was this helpful?
What can we do to improve the information ?