Technical FAQs

Ask a Question

What is the difference between the QO24L70RBCP and the QO24L70RB load centers

Issue:
Product Features

Product Line:
QO LC

Cause:
Clarifying product features differences

Resolution:
The difference is the packaging. The CP suffix indicates a product with retail type of packaging. Other than the packaging they are the same device.


CTA-ID : 2029759
Was this helpful?
What can we do to improve the information ?