Technical FAQs

Ask a Question

What is the part number of the keypad and the remote mounting kit for the Altivar ATV58 drive?

Issue:
What is the part number for the keypad and the remote mounting kit for the Altivar ATV58?

Product Line:
ATV58

Environment:
All

Cause:
NA

Resolution:
VW3A58103 is the part number for the kit. This kit includes the mounting hardware and a 3 meter cable. It does not include the keypad itself. The keypad is VW3A58101U.
However, both part numbers are obsolete and there is no direct replacement.
Was this helpful?
What can we do to improve the information ?