Technical FAQs

Ask a Question

Is the SN1200NACT provided with a neutral CT?

Yes, the SN1200NACT is provided with a NE12CT2 neutral CT as an integral element of the neutral assembly.


CTA-ID : 2029859
Was this helpful?
What can we do to improve the information ?