Technical FAQs

Ask a Question

9421LN1: Can the handle be changed to a Stainless Steel handle?

Stainless steel not available. Suggest the 9421LC46 which is for NEMA 3, 4, 4X and is chrome plated.


CTA-ID : 2029776
Was this helpful?
What can we do to improve the information ?