Technical FAQs

Ask a Question

AL250LA lug. What is the torque specification of the lug mount to the breaker? What is the wire binding screw torque?

Mounting torque is 80 in. lbs. Wire binding screw torque is 375 in. lbs.

CTA-ID : 2029742
Was this helpful?
What can we do to improve the information ?