Technical FAQs

Ask a Question

When using the 0-10VDC AI2 analog input the drive goes to the 60Hz HSP setting when 5VDC is applied to the input rather that going to 60Hz at 10VDC.

If the Fr1configuration of reference 1is programmed as AI2 and since the SA2 summing parameter is factory set to AI2 this input will sum with itself giving 60 Hz at 5VDC rather than 10VDC. Program SA2 from the ``AI2`` setting to the ``No`` not assigned setting to correct this problem.

CTA-ID : 2029860
Was this helpful?
What can we do to improve the information ?