Technical FAQs

Ask a Question

Will an FA34100G type breaker with a GFM100FA type ground fault module fit in an HCM type I-Line panel?

No. The HCM panel accepts a maximum 250A, KA frame size breaker. The combination of an F frame breaker and a GFM100FA ground fault module takes up the same space as an LA frame breaker. The combination of an F frame breaker and a GFM100FA ground fault module is physically too long to fit in an HCM panel, since there would be no wire bending space left.


CTA-ID : 2029789
Was this helpful?
What can we do to improve the information ?