Technical FAQs

Ask a Question

Are the copper compression lugs made of copper material? Do the copper compression lugs accept aluminum and copper conductors?<br />

Copper compression lugs are made of copper and may accept copper conductors only, or copper and aluminum. Read the footnotes below the listing table.


CTA-ID : 2029746
Was this helpful?
What can we do to improve the information ?