Technical FAQs

Ask a Question

What is the replacement for an HCN2754-1MN I-Line panelboard interior?<br />

Use a HCN27741MN. It has the same amount of branch mounting space and will fit in the old 54`` high box. However, the original trim will not fit there are no replacement trim is available.


CTA-ID : 2029728
Was this helpful?
What can we do to improve the information ?