Technical FAQs

Ask a Question

Is replacement control coil available for 8910DPA123V06?

31074-400-57 for 480v/60 hertz and 440v/50 hertz applications, coil consumption is 700 VA inrush, 46 VA sealed for 60 hertz applications or 678 VA inrush, 47 VA sealed for 50 hertz applications.

CTA-ID : 2029771
Was this helpful?
What can we do to improve the information ?