Technical FAQs

Ask a Question

Is there an adapter kit to put an QO interior in a MH** panelboard box?

Issue:
Is there an adapter kit to put an QO interior in a MH** panelboard box?  

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Panelboard enclosures and QO load center sold and supported in the USA.

Cause:
Adaptor for retrofitting a QO load center in a panelboard enclosure.

Resolution:
We do not offer an adapter to mount a QO load center in a panelboard enclosure.








CTA-ID : 2029744
Was this helpful?
What can we do to improve the information ?