Technical FAQs

Ask a Question

Is the main breaker included in the RC2M200S and RC2M200SH CSED Meter-Mains device?

Issue:
Application

Product Line:
CSED

Environment:
Application

Cause:
Verification

Resolution:
The main breaker(s) are not factory installed in the RC2M200S, nor RC2M200SH. They must be ordered separately. The primary main accepts a QOM2-VH type, 200A maximum. The secondary main accepts a QO-VH type, 50A maximum.


CTA-ID : 2029970
Was this helpful?
What can we do to improve the information ?