Technical FAQs

Ask a Question

How many fuses are needed for a fusible safety switch?

Issue:
Product Design Features

Product Line:
General Duty, Heavy Duty and Double throw safety switches

Environment:
Fuses

Cause:
Installation

Resolution:
That would depend on the exact catalog number of the fusible switch and how many switching poles the switch contains.  A 2-pole fusible safety switch would require one fuse per switching pole, so 2 fuses OR a 3 pole fusible safety switch would require one fuse per switching pole, so 3 fuses etc.



CTA-ID : 2029701
Was this helpful?
What can we do to improve the information ?