Technical FAQs

Ask a Question

What is the quick connect cable is used for the XUVK0252VS and XUVK0252S photo sensors?

These sensors require the M8 3-pin connector. The suffix ``S`` always codes for the pico style M8 connector. Use part number XSZCS141 for 5 meter straight connector and XSZCS151 for the 90 degree connector. See information on pages 524-525 of the Solid State Sensors catalog #9006 CT0101.

CTA-ID : 2029831
Was this helpful?
What can we do to improve the information ?