Technical FAQs

Ask a Question

What are the storage requirments for thermal-magnetic circuit breakers?

Circuit breakers should be stored in a dry, ventilated room, protected from dust, rain, water and chemical agents. If storage is for an extended period, the relative humidity in the room must be maintained below 70%, and temperature must be in the range of -40ᄚC +85ᄚC.


CTA-ID : 2029781
Was this helpful?
What can we do to improve the information ?