Technical FAQs

Ask a Question

What hole size or KO is needed for a PK6FL.

The mounting hole or KO has a concave shape with two flats on the sides and a doomed top/bottom. From top to bottom the hole is one (1) Inch, and from side to side the hole is 5/8 Inch.



CTA-ID : 2030015
Was this helpful?
What can we do to improve the information ?