Technical FAQs

Ask a Question

Where can the ampere rating be found on QO and QOB breakers?

Usually, the amperage is only indicated on the handle of the breaker. Some QOB breakers have a bar code sticker with the breaker catalog number affixed to the rear of the breaker.

CTA-ID : 2029834
Was this helpful?
What can we do to improve the information ?