Technical FAQs

Ask a Question

What are the enclosure ratings for the XVP Indicating Banks?

The XVP Indicating Banks are rated IP65, Nema Type 1, 12 and 13


CTA-ID : 2029799
Was this helpful?
What can we do to improve the information ?