Technical FAQs

Ask a Question

What is the classes of NEMA 9 for Combination Starters

Issue:
What is the  classes of NEMA 9 for Combination Starters

Product Line:
Nema combination starters sold and supported in the USA.

Environment:
Definition

Cause:
Application

Resolution:
Combination Starters in NEMA 7 & 9 enclosures for Hazardous Locations cover Class I, Groups C and D; Class II, Groups E, F and G; Divisions 1 and 2

Revision:
 Effective 2011, the Nema 7 and 9 enclosures for combination starters are no longer available and we offer no substitute for them. 


CTA-ID : 2030294
Was this helpful?
What can we do to improve the information ?