Technical FAQs

Ask a Question

What are the storage requirments for the Masterpact NW and NT circuit breakers?

Masterpact circuit breakers should be stored in a dry, ventilated room, protected from dust, rain, water and chemical agents. If storage is for an extended period, the relative humidity in the room must be maintained below 70%, and temperature must be in the range of -40ᄚF (-40ᄚC) to 185ᄚF (85ᄚC).
The breakers must be stored in the open (OFF) position with the charging springs discharged.

CTA-ID : 2029784
Was this helpful?
What can we do to improve the information ?