Technical FAQs

Ask a Question

Can I get a field installed neutral for a double throw safety switch catalog number 82254?

No. There is no kit available to field install a neutral to this switch. If a neutral is needed, catalog number 82254N must be ordered instead.

CTA-ID : 2029753
Was this helpful?
What can we do to improve the information ?