Technical FAQs

Ask a Question

Did ANY of the Intelligent Load Center(ILC) catalog numbers include the Automatic Transfer Switch, control panel and other components?

Issue:
Product Design Features

Product Line:
QO Load Centers 

Environment:
Automatic transfer Switch and control panel

Cause:
Application

Resolution
NOTE: ALL the ILC catalog numbers have been obsoleted and are no longer available with no replacements.

But, No the automatic transfer switch(ATS), control panel, other components required and generator were sold through Kohler Power System Distribution. The ILC load centers that came from Square D, ONLY came with provisions for ALL the generator application components to be installed and the load centers were only sold through Square D - Schneider Electric Distribution.



 
Was this helpful?
What can we do to improve the information ?