Technical FAQs

Ask a Question

What is the magnectic setting for the 250 Amp JG breaker ?

The low setting is 1250 A; the high setting is 2500 A.


CTA-ID : 2030296
Was this helpful?
What can we do to improve the information ?