Technical FAQs

Ask a Question

Is NS100/160/250 a good part number?

This is shorthand for designation of circuit breaker types NS100 NS160 and NS250 which are IEC versions of the Compact NSF breaker. More information is needed to select a breaker and determine catalog number. Select from MG Pricing Guide.


CTA-ID : 2030413
Was this helpful?
What can we do to improve the information ?