Technical FAQs

Ask a Question

What is the part number for the mounting screws of the Powerpact J frame breaker?

Issue:
Need screws for mounting Powerpact H or J Frame breakers

Product Line:
Circuit Breakers

Environment:
Powerpact H or J Frame breakers

Resolution:
The parts bag kit number is 48200-236-50. It contains (2) 8-32 X 2.62 panhead screws.




 
Was this helpful?
What can we do to improve the information ?