Technical FAQs

Ask a Question

Are the H328N, H328NAWK and H328NR suitable for use as service entrance equipment?

Issue:
Application

Product Line:
HD Safety Switch

Cause:
Application 

Resolution:
Yes, these safety switch will be marked: "Suitable for use as service equipment". To be used as service equipment the neutral assembly should be bonded to the enclosure with the bonding assembly provided with the switch.



CTA-ID : 2029959
Was this helpful?
What can we do to improve the information ?