Technical FAQs

Ask a Question

Can a HOM2100 be used as a main breaker in a RC816D200CH CSED?

No, it cannot. The factory installed 200A main breaker, HOM2200, is four poles wide and is fed by four ungrounded conductors from the load side of the meter socket. The HOM2100 is only two poles wide, so there is no way to terminate the four conductors from the meter socket.


CTA-ID : 2029826
Was this helpful?
What can we do to improve the information ?