Technical FAQs

Ask a Question

What type of hub is used on the UT2R2122B horizontal ganged meter socket?

Issue:
Selection

Product Line:
Horizontal Meter Socket

Cause:
Accessory selection

Resolution:
The UT2R2122B has a hub opening in the top endwall, designed to accept Type "A" hubs. Type "A" hubs are available to accept 1" through 2 1/2" conduit.
1" = A100
1.25" = A125
1.5" = A150
2" = A200
2.5" = A250


CTA-ID : 2029975
Was this helpful?
What can we do to improve the information ?