Technical FAQs

Ask a Question

What is the catalog number for the standard four auxiliary contacts for the Masterpact MP breaker?

Issue:
What is the catalog number for the standard block of four auxiliary contacts for the Masterpact MP breaker?

Product Line:
Masterpact MP

Resolution:
The new number for the contacts is 54525.  The old obsolete number was 685725.
It has 4 normally open and 4 normally closed contacts.

 
Was this helpful?
What can we do to improve the information ?