Technical FAQs

Ask a Question

GS1GU3: Can the switch be flipped and mounted upside down?

No. It was not designed for that purpose. Lettering would be up-side down, line and load terminals will be reversed, and will void UL listing. If the customer knows that the switch needs to be inverted, they can order the part GS1GU3S02 which will have the lettering and terminals reversed.

CTA-ID : 2029774
Was this helpful?
What can we do to improve the information ?