Technical FAQs

Ask a Question

Are the aluminum labeled compression lugs actually made of aluminum material? Do the aluminum compression lugs accept aluminum and copper conductors?

Lugs for Transformers

Product Line:
LV Transformers

Applies to Low Voltage Transformers by SquareD/Schneider Electric

Transformers over 15 KVA have terminals that require lugs

Aluminum compression lugs are made of aluminum and accept either aluminum or copper conductors, unless otherwise indicated.

CTA-ID : 2029745
Was this helpful?
What can we do to improve the information ?