Technical FAQs

Ask a Question

Can 9037DW6Z5 and a 9038JW6Z5 be provided with 316 stainless steel collars and a ground post & cross tie ?

The Z5 indicates all wetted parts including the collars , post & tie , are stainless . The flange, however, is not stainless.
***** Reised from resolution 1457 Added key words *****

CTA-ID : 2030445
Was this helpful?
What can we do to improve the information ?