Technical FAQs

Ask a Question

Are the Class 8536 Type S starters available with dual voltage coils?

No. Dual voltage coils are NO LONGER available on NEMA sizes 0, 1, 2, 3 (excludes sizes 2 & 3 with 4 and 5 poles) only. The appropriate voltage code had to be used along with Form Y5. The following were the available voltages with required code:

115/230 volt 60 hertz - code V99 (specify 115/230 volt 60 hertz)
115/230 volt 50 hertz - code V99 (specify 115/230 volt 50 hertz)
120/240 volt 60 hertz - code V33
240/480 volt 60 hertz - code V34


CTA-ID : 2030420
Was this helpful?
What can we do to improve the information ?