Technical FAQs

Ask a Question

Do we market 2-pole or 3-pole QO or QOB breakers with a higher inrush capability?

Issue:
Do we market a QO3100HM with a higher inrush capability?

Product Line:
QO

Environment:
Minature Circuit Breakers

Cause:
Catalog Selection

Resolution:
No, we do not market a "high inrush" QO or QOB breaker with 2 or 3 poles because they are high magnetic as standard. The high magnetic type QO breakers (with HM suffix) are limited to single pole and 15 or 20A amperages. All other amperage and pole configurations are high magnetic as standard, with no special suffix required to get this feature.

Please use our breaker trip curves to verify a specific breaker will work for your application.
Was this helpful?
What can we do to improve the information ?