Technical FAQs

Ask a Question

Is the SU3040D400CB provided with a factory installed service disconnect?

Issue:  
What is the main disconnect that comes installed in all-in-one SU3040D400CB?

Product line:  
Combination Service Entrance Devices (CSEDs)

Environment:  
All-in-One Square D CSEDs

Resolution:  
Yes, a QDL22200 is supplied factory installed.  The factory installed QDL22200 feeds the 30 space/40 circuit load center interior.  Additional space is provided for the field installation of a second QDL main breaker, 200A maximum.
Was this helpful?
What can we do to improve the information ?