Technical FAQs

Ask a Question

What is the terminal data for the GJL circuit breaker (Ex: GJL36020, GJL36100)?

The lug will accept one #14-1/0 AWG Copper or one #8-1/0 AWG aluminum.


CTA-ID : 2030519
Was this helpful?
What can we do to improve the information ?