Technical FAQs

Ask a Question

Are NF panelboards rated for use at 400 Hz?

Issue:
Are NF panelboards rated for use at 400 Hz?

Product Line:
NF Panelboards

Environment:
Application

Cause:
Clarification

Resolution:
Yes. NF panelboards are rated for 400 Hz.
The circuit breakers must be rerated for 400 Hz applications.  See 0100DB0101 for rerating information.


CTA-ID : 2030495
Was this helpful?
What can we do to improve the information ?