Technical FAQs

Ask a Question

Is it possible to install a 400A fusible plug-in unit on to 225A busway? The customer is trying to feed a motor with very high inrush and about 200A running current, and wants to use a physically larger fuse style.

Yes, the plug in unit will fit. The plug in unit needs to be supported externally by a separate drop rod. The jaw is compatible. Take care not to draw more than the rated amperage of the busway.

CTA-ID : 2029905
Was this helpful?
What can we do to improve the information ?