Technical FAQs

Ask a Question

Is the SC2040M200C provided with a factory installed service disconnect?

Issue:
Product Features

Product Line:
CSED

Cause:
Clarifying if a main breaker disconnect is provided

Resolution:
Yes, a HOM2200 is provided as a back fed main breaker disconnect, factory installed.


CTA-ID : 2030511
Was this helpful?
What can we do to improve the information ?