Technical FAQs

Ask a Question

What is the catalog number for a plug-on, 125A, three phase, sub-feed lug kit for a QO load center?

Issue:
What is the catalog number for a plug-on, 125A, three phase, sub-feed lug kit for a QO load center?

Product Line:
QO 3 Phase Load Centers, QO Breakers

Environment:
QO 3 Phase Load Center or NQ Panelboard

Resolution:
The Catalog number is QO3125SL.

Note:  125A is the large sub feed breaker amperage available in QO.

CTA-ID : 2029830
Was this helpful?
What can we do to improve the information ?