Technical FAQs

Ask a Question

Will NQOD main lug panelboards still be UL approved if VCEL type compression lugs are used to feed it?

Yes. The panels do maintain their UL listing when they are fitted with compression lugs.


CTA-ID : 2030452
Was this helpful?
What can we do to improve the information ?