Technical FAQs

Ask a Question

Can a ZB4BV05 or similar Incandescent/LED pilot light head be used with a ZB4BVG5 or similar Protected LED light module with collar ?

No ... the standard ZB4BV05 head is too short to accomodate the LED bulb in the base . The ZB4BV05 should be used with a ZB4BV6
ZB4BVG5 is used with protected LEDs

CTA-ID : 2030276
Was this helpful?
What can we do to improve the information ?