Technical FAQs

Ask a Question

What are the repair parts for a QU816D400CK, Series M01?

Issue:
Design repair parts 

Product Line:
Combination Service Entrance Devices 

Environment:
Repair parts

Cause:
Maintenance

Resolution:

NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.

Only the parts listed below are considered field replaceable.
Meter Cover - 4056247750. This is a one piece Meter Cover/Utility Pullbox Cover.
Meter Cover Mounting Screws 4020513001K and (3) Sealing Screw X1299
Load Center Cover - 4056258950
Load Center Cover Mounting Screws - (3) 2142217101
Utility Pullbox Cover - See Meter Cover, above.
Utility Pullbox Cover Handles - The Meter Cover is not supplied with handles.
Load Center Interior - 4056259350
Load Center Interior Mounting Screws - (4) 2142217101
Load Center Interior Lugs - (2) 4025116051 and Keps Nut (2) 2342702000
Interior Deadfront Trim - 4056233101
Interior Deadfront Trim Mounting Screws - 4020513001K
Meter Base Assembly - 58763-4 and 58764-4
Mounting Channel - 4056142003
Factory Installed Main Breaker - QDL22200
Utility Lug Mounting Hardware - 4056211850
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.


CTA-ID : 2030267
Was this helpful?
What can we do to improve the information ?