Technical FAQs

Ask a Question

Will the lever arm on XCKJ10511 spring back to the center position?

Yes, wherever that lever starts, it will spring back to that position.


CTA-ID : 2029935
Was this helpful?
What can we do to improve the information ?