Technical FAQs

Ask a Question

How do you activate the ground fault protection feature on a Masterpact or Powerpact breaker with a 6.0 A Trip unit?

Issue:
How do you activate the ground fault protection feature on a Masterpact or Powerpact breaker with a 6.0 A Trip unit?

Product Line:
Micrologic, Powerpact, Masterpact

Environment:
Products sold in North America

Cause:
Need to remove ground fault from breaker with a LSIG trip functions.

Resolution:
The ground fault cannot be deactivated. The trip unit needs to be replaced to an unit without LSIG trip functions like S143A (5.0A).

CTA-ID : 2030439
Was this helpful?
What can we do to improve the information ?