Technical FAQs

Ask a Question

PXF361600G -- Customer is wanting to know adjustment range for the ground fault settings.

The ground-fault pick up and the ground fault delay are adjustable from 20% to 75% of the sensor.


CTA-ID : 2030469
Was this helpful?
What can we do to improve the information ?